The BioPAT® Conductivity | pH single-use pipe can be ordered in different sizes, various connections and different set-ups, depending on the desired application.
The single-use pipe mainly consists of the single-use pipe itself, the conductivity sensor which is already pre-installed and a pH electrode (wet stored) which is either already connected to the pipe or can be assembled optionally.