Our eShop will be on maintenance from May 15th 2026, 3:00 PM until May 17th 2026, 10:00 PM CEST. Please note that during this time the eShop will be available with limited functionality only.

BioPAT®Fundalux is an absorption-based photometric probe that uses light from 840nm to 910nm to measure the turbidity in bioreactors and fermenters. A precisely defined and constant LED light beam passes through the process medium from either side of the gap on the probe’s shaft.

  • Designed for use in R&D, as well as in pilot- and production-scale

  • Monitoring cell growth in bacterial fermentation and mammalian cell cultures.

  • Online triggering of control loops for advanced automated fermentation.

See more Products below
*Custom/bulk order quotes are provided within 72 hours of request.
BioPAT® Fundalux
BioPAT® Fundalux

BioPAT®Fundalux is an absorption-based photometric probe that uses light from 840nm to 910nm to measure the turbidity in bioreactors and fermenters. A precisely defined and constant LED light beam passes through the process medium from either side of the gap on the probe’s shaft.

  • Designed for use in R&D, as well as in pilot- and production-scale

  • Monitoring cell growth in bacterial fermentation and mammalian cell cultures.

  • Online triggering of control loops for advanced automated fermentation.

Item No.:
BioPAT_Fundalux

Overview

Specifications

Choose your product

Filter by product attributes

Products (16)

Results per page: | |

The turbidity measuring system BioPAT® Fundalux is based upon measuring the attenuation of the intensity of light brought about by the process medium by use of a high precision single channel absorption photometer.

The measurement range is 0 – 6 AU (Absorbance units). Its hermetically sealed photodiode detects attenuation of light intensity, which is caused when light is absorbed by cellular mass, dissolved compounds and insoluble material. The 180° constant direct beam optical path lengths (OPL) allow maximum utilization of LED light intensity.

The changes in detected light intensity are caused by different degrees of absorption by materials in the medium, which is described by the Beer-Lambert law. This states that the logarithm of the transmission loss is proportional to the concentration of a substance.

In addition, as BioPAT®Fundalux operates according to the transmittance principle in the range, it is not affected by color changes in the cultivation medium. As a result, the probe measures the concentration of total biomass accurately and constantly throughout a process based on the respective medium properties.

Applications

  • Application
    Process Analytical Technologies (PAT)
  • Usage
    Multi-use

Features

  • Device/Instrument Compatibility
    • Univessel® Glass
    • Steelvessel

Product Information

  • Brand
    BioPAT® Fundalux